AOUT#.CUTOFF
Description
AOUT#.CUTOFF sets the cutoff frequency in Hz for a single-pole low-pass
filter on the Analog Output.
A value of 0 Hz will turn off the filter and will allow all frequencies to pass through.
The filter can be used with all modes of Analog Output.
Examples
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | Hz |
| Range | 0 to 10,000 Hz |
| Default Value | 0 Hz |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.